This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340 12V升20V 芯片烧毁

Other Parts Discussed in Thread: TPS55340

故障现象:

1、55℃老化后,TPS55340的SW脚对地短路,测试电感到SW脚的电流,发现电路不论电流大小,一直工作在断续模式,峰值电流10A以上。用电子负载缓慢增加负载电流0.1~1A,TPS55340也不能切换到连续模式,超过负载超0.7A后很容易烧毁,烧毁现象是SW脚对地短路。

2、找到1pcsTPS55340能够工作在连续模式的板子,与故障板电路对比无差异(同一批次生产),交叉验证TPS55340,工作方式不跟随芯片走。

求问:TPS55340的为什么不能切换工作模式? 附件是详细测试报告。

请各位大神指教,感谢!

          

TPS55340烧毁问题分析报告.docx