This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24133充电失败,LED常亮显示异常

Other Parts Discussed in Thread: BQ24133

中午好:

      关于BQ24133充电你们都解决了吗?12V/3A Adapter单独供电,电池(2节串联18650可充电锂电池)单独供电和电池与Adapter同时接入,系统供电正常,但充电失败,LED一直常亮异常。焦虑定位花费很多精力,恳请赐教,欢迎来电(18061693530 张工)指导,万分感谢!!!

1.电池无论插上与否,LED常亮,调整过Charge输出电容(10uF以下),LED灯还是常亮。

2.电池插上LED灯亮,测试发现实际并未充电

另有疑问:测试发现只要Adapter接入,BATFET都是关断,BATFET仅用于电池单独接入充当放电回路,给系统供电用吗?充电不需要外部BATFET通路,是否仅靠内部集成MOS通路即可充电?

电压测试情况:

单位/V 单独12V/3A Adapter Adater和电池同时接入 仅电池(2节串联18650)
AVCC 11.6 11.6 7.5
CMSRC 12 12
ACDRV 18 18
VREF 3.3 3.3 0
ISET(参数调整R364=20K) 0.2 0.2 0

ACSET(参数调整R370=330K,R369=220K)

1.305 1.305 0
OVPSET 1.105 1.105
TS(参数调整R367 20K) 1.98 1.98 0
BATDRV 12(BATFET关断) 12(BATFET关断) 0.98(BATFET导通)
RGEN 5.98 5.98
BTST 5.41 5.41
SRN 7.5 7.5
SW 7.5 7.5

VSYS2---VSYS之间电路为实现理想二极管功能,BATT2_GND通过0欧姆电路接地。

上述原理图截图参考手册与Demo,测试时做过如下调参:

1.ISET(参数调整R364=20K),同时将R108有10毫欧调整为20毫欧。Icharge=0.2/20*0.02=0.5A=500mA。看电池包原装充电器上显示12V/600mA输出,原装如此,担心大于600mA充电电流电池自锁(仅个人认为),估调小充电电流。另1A充电电流时现象一样的

2.ACSET(参数调整R370=330K,R369=220K)同时将R176有20毫欧调整为10毫欧。原稿(Demo和手册)参数Vacset=0.6V,Isupply Max=0.6/20*0.02=1.5A;寻思增大供电电流(Adapter为12V/3A),调参后Isupply Max=1.3/20*0.01=6.5A;保持原参数Isupply Max=0.6/20*0.01=3A。此处无论怎么调参,用Adapter还是稳压电源供电,现象均一样。

3.TS(参数调整R367 20K)。原稿(R367=5.6K),Vts=2.78V,查阅手册在温度门限以外,估做此调参,测得Vts=1.98V。注:Vts=2.78V门限以外时,LED灯一直闪烁(除了电池单独供电Sleep,LED熄灭);调参Vts=1.98V满足温度门限,LED灯常亮(除了电池单独供电Sleep,LED熄灭);此处调参LED状态有变化。

充电条件一一排查过满足要求。