out project designed main board not same to EVM, it diffcult to generate current 0 load and current 1000mA load.
but now i need calibrate my board include bq35100, without current 0,
I try it , but the bqstudio report:Calibration- Current flow across sense resistor, Please ensure no current is flowing and retry calibration.
how can I calibrate CC Offset/Board Offset?
my battery is Li-SOCl2, use bq35100 to detect soh.
thank you!
使用BatteryManagementStudio 校准CC Offset/Board Offset时候,一直提示Calibration- Current flow across sense resistor, Please ensure no current is flowing and retry calibration.
我们自己的项目不是 EVM。0负载和1000mA的固定负载很难做。
Verify whether the Current reports 0 mA. Proceed with the Board Offset Current calibration of current is
reported.
Connect a 1-A load from BAT+ to PACK–
这2种条件很难实现。
请问我们自己设计的项目在bq35100上如何校准CC Offset/Board Offset/current 校准?
我们使用的是锂亚电池。Li-SOCl2
谢谢!