This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq35100 how to CC Offset/Board Offset Calibration?

Other Parts Discussed in Thread: BQ35100, BQSTUDIO

out project designed main board not same to EVM, it diffcult to generate current  0 load and current 1000mA load.

but now i need calibrate my board include bq35100, without current 0,

I try it , but the bqstudio report:Calibration- Current flow across sense resistor, Please ensure no current is flowing and retry calibration.

how can I calibrate CC Offset/Board Offset? 

my battery is Li-SOCl2, use bq35100 to detect soh.

thank you!

使用BatteryManagementStudio 校准CC Offset/Board Offset时候,一直提示Calibration- Current flow across sense resistor, Please ensure no current is flowing and retry calibration.

我们自己的项目不是 EVM。0负载和1000mA的固定负载很难做。

Verify whether the Current reports 0 mA. Proceed with the Board Offset Current calibration of current is
reported.
Connect a 1-A load from BAT+ to PACK–
这2种条件很难实现。

请问我们自己设计的项目在bq35100上如何校准CC Offset/Board Offset/current 校准?

我们使用的是锂亚电池。Li-SOCl2

谢谢!