This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020 高温老化时出现出现内部L1(PIN8,PIN9),对地短路现象

Other Parts Discussed in Thread: TPS63020

现象:

     TPS63020 高温老化时出现出现内部L1(PIN8,PIN9),对地短路现象,EN脚是MCU控制,常温下状态正常,设备正常,当环境温度TA>70℃以后,出现L1对地短路,电路原理参照手册设计:

使用示波器测试时,发现程序在控制使能的时候,存在MCU指令中有T1=100uS和T2=10mS的EN拉低电平,这样是否会使芯片在降压模式下,误认为未关机,丢周期,造成占空比过小,续流mosfet通流过大,造成芯片损伤?目前3套样品中出现2套,均在高温下L1对地短路。请尽快回复,谢谢

  • 首先环境温度为70度,你可以简单计算下当前芯片功耗,计算下结温是多少,如果结温临近芯片规定值,则芯片内部有没有过热保护就是一个问题,温度很高时,内部异常很正常。

    再就是EN脚为低电平,应该是芯片未使能,且Vin还存在,所以进行反向Buck的情况不现实;(你可以向技术支持确认在EN为低时,Vin有电,芯片下管是什么状态,我认为是关断的,不导通);

    有条件要测试下L1两端电压、电流波形,这样看起来更直观一些;
  • 首先,谢谢您的回复,TPS63020手册中

    具有安全可靠的操作特点–过热、过电压保护,而且负载工作在周期模式下,1min 周期,工作5S,整个温升不会超过10摄氏度,各个测试点的电压波形在室温条件下测试均正常,无异常尖刺现象。