This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1无法真正进入SHUTDOWN或者进入SHUTDOWN后无法正常退出

Other Parts Discussed in Thread: BQ40Z50-R1, EV2400

老师,你好;

我在使用BQ40Z50-R1是发现一个问题,当通过 the gauge is sealed and the MAC Shutdown() command is sent twice in a row方式进入SHUTDOWN时,偶尔会出现问题,问题如下:

正常情况下,连续发送两次指令后,BQ Studio上首先出现SDM标志位由绿色变为红色,然后XCHG和XDSG标志位由绿色变为红色,然后真正进入shutdown(BQ studio无法与BQ40Z50-R1进行通讯);然后给电池组充电正常退出SHUTDOWN

异常情况下,连续发送两次指令后,BQ Studio上首先出现SDM标志位由绿色变为红色,然后XCHG和XDSG标志位由绿色变为红色,一直无法真正进入shutdown(BQ studio仍然与BQ40Z50-R1进行通讯,如下图所示);然后给电池组充电也无法正常退出SHUTDOWN;需要等带大约30分钟(时间不一定),才能真正进入shutdown(BQ studio无法与BQ40Z50-R1进行通讯);然后给电池组充电正常退出SHUTDOWN

备注:1、我们使用BQ40Z50-R1大约有3年时间了,有5款不同的产品,不同的产品上都不时会出现此问题;

2、通过发送指令进入shutdown出现过此问题、通过AUTOSHIP功能自动进入shutdown也出现过此问题;

问题:造成上述问题的原因是什么呢,该如何处理

x 出现错误。请重试或与管理员联系。