This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50 max error问题

  Max error有两项设置Time Cycle Equivalent和Cycle Delta,我都是使用的默认值24h和0.05%,于是当学习完成后max error=1%,随着静置时间越长,max error会发生变化,大约一个月到2%,两个月到4%,请问这个会影响电量精度吗?还是需要重新学习,或者cycle delta改为0,这样就会一直保持在1%。

  • Max error can change if passed charge exceeds a cycle count threshold and your conditions do not allow for a Qmax update. For every cycle without a Qmax update Max error will increase by cycle delta
    不会影响精度,您可以通过学习重新update Qmax and Ra max error就会回复1%
  • 那这两个参数设置有什么用啊?学习成功后可以直接将cycle delta设置为0,这样就不会变化了啊
  • Each increment of CycleCount() after valid QMax update will increment of MaxError() by Cycle Delta. Setting this parameter to 0 disables the MaxError() increment by time or cycle increment.
    充放电过程中cycle count增加,max error会增加,如果 您不需要这个功能可以设置Cycle Delta 0来取消这个功能。