This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180,设计一个1550W的的APFC,遇到了问题。



如题。现在样机做出来了。输出电压385V,输入AC176-256V,功率1550W。

按照TI提供的Excel表格计算的。计算到最大占空比是0.354,但是在实际电路中,在正弦波接近零点的时候,最大占空比去到了0.8左右了。而此时测试负载才400W左右,输入电压AC220V,这个正常吗?

下图为输入AC220V,负载400W时候的波形图。红色为MOS管G-D电压波形。蓝色为MOS管D-S电压波形。此刻是正弦电压过零附近的波形。此时功率因素为0.99,电压THD为1%,电流THD为9%。