This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于12V转5V的Buck方案,TPS5405输出有震荡的问题

Other Parts Discussed in Thread: TPS5405

TI的老师,你们好。我在测试TPS5405的过程中发现了如下问题:

  1. 输出空载时,输出电压是阶梯上升的设定输出电压5V的。(输入12V,输出设定为5V)图1
  2. 输出带载时,输出电压和电流会震荡,然后再进入稳定的输出模式(负载电流约为500mA)。图2

我的问题是:这种情况是否是正常的,如果不正常,是什么原因导致的?

测试条件:开关频率设定为560KHz,输入电压为12V,输出为5V,输入电容为47uF,输出电容为22uF.

波形如下:

图1

图2