This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650 充电时电感发热

Other Parts Discussed in Thread: BQ24650

最近在折腾BQ24650,输入18-21V 。输出14.3V给铅酸电池充电。现在电感是4.7uh ,MAPM1040F-4R7M-LF,4.7uH,11.8*10.8*4.0mm,±20%,16.5mΩ,Isat=13A,Irms=8A.采样电阻是5毫欧,输入电压是18DC/5.1A的稳压源。在18V 5A输入时,约6A的充电电流。现在的问题是电感发热,导致整个板子也发热。充电一会后,输入电源的电流会一直下降。主要是这个电感换成同规格的3.3uh的,也换过11.8*10.8*5.8的。也是会发烫。

  • 6A充电电流,有没有算过电感的电流峰值及有效值?是不是余量太小了。而且充电后输入电源电流下降是怎么回事?是电池满了还是电感值降低峰值电流增大造成过流保护了?我的意见是选择更低ESR更大电流值的电感。