This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请求BQ24773RUYR第一次上电不能充电问题



各位BOOS,

此项目是蓝牙音箱,型 号TS4300,所用电池容量2475mAH,

一、整机按电源键开机,进入工厂测试模式,插入232串口,插入AC进入自动化测试,第一次上电充电电流不正常,但电量及温度能检测,把机器断电,拔电池后,再插电池,插AC上电,此时充电正常,

二、测量不良品IC管脚数据如下

1、电池不充电有两种不良状态(正常关机充电电流1.2A左右,开机充电电流630mA左右)
a、整机插入AC电源,电池充电电流0mA
b、整机插入AC电源,电池充电电流300mA(电流不良有几种,100-350mA之间)

2、24773管脚测量如下(电池电量在7.5V左右)
a、充电电流在0mA时,18脚BATDRV输出电压0V,L104电感电压7.5V,
     23脚LODRV输出电压0.25V,,26脚HIDRV输出电压9.0V,
b、充电电流在100mA-350mA时,18脚BATDRV输出电压7.45V,L104电感电压8.25V左右,
     23脚LODRV输出电压0.75V,,26脚HIDRV输出电压9.0V,

电路图如下: