This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23861无输出,I2C读取地址正常。

Other Parts Discussed in Thread: TPS23861

       我司应用在高压塔(1000KV高压塔)现场返回的6套设备均出现POE无输出故障(其它通信功能完全正常,其它器件也没有损坏现象,只更换TPS23861后设备PSE对外供电恢复正常),经检测,CPU与2片TPS23861之间的I2C通信均正常,可以读取寄存器数据。示波器测量芯片GATE1~4均无输出波形,原理图完全参考DEMO设计。
 
异常设备的寄存器数据与正常设备的数据进行了对比,发现POE失效设备的自动探测功能不生效,现象为不对外供电。
POE工作模式为Auto。
 
失效设备的此项寄存器读数为0x0
正常工作设备此寄存器读数为0xF(对应4个端口)
 
 
  • Hi
    见datasheet描述:
    The TPS23861 will not automatically apply power to a port under the following circumstances:
    • The detect status is not Resistance Valid.
    • If the classification status is overcurrent, class mismatch, or unknown.
  • 已经确认不是此两种情况引起的TPS23861无输出,我们更换过确认正常的PD也是同样的现象,不良设备更换TPS23861芯片后正常,将换下的不良TPS23861芯片换到原本好的板上也同样会出现无输出,所以确认为TPS23861芯片损坏了,但是因为什么损坏没有找到原因,由于设备是在特殊场景(1000KV高压塔上)应用,所以需要帮分析下TPS23861芯片在什么情况下会出现此类故障,如果是雷击浪涌损坏TPS23861芯片表面应该会有烧毁痕迹(不良芯片没有任何烧毁痕迹),对比测试TPS23861芯片对地阻值也与好的芯片一致。
  • Hi
    如果是要确认芯片哪里不良,最好是开壳来看,TI这边应该是有这类分析,应该是需要自费的。你可以联系你购买芯片的渠道,让他们告诉你渠道。(我这边是在线的,也没有这个渠道信息)