This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3424 DIM引脚通过PWM调光接线

Other Parts Discussed in Thread: LM3424

请问:
    LM3424 DIM引脚通过PWM调光接线

   PWM信号是直接 接入nDIM引脚,还是接入到R4电阻的左边 (如下图)

   还是说当接入PWM信号后,就不需要R4电阻了。PWM信号可以直接 接入nDIM引脚。

   麻烦协助。

   此处PWM应该是电压型的吧。

     

  • HI
    见datasheet第29页,在nDIM脚给PWM信号调光。
  • 你好

      问1: 如果使用PWM调光,占空比最大97%,这样会影响CSH脚位电压吗?

                目前测试如果不用PWM调光,电压可以1.23-1.24V之间,如果接入PWM调光 CSH脚位电压就成1.15V左右。

      问2:    在不使用PWM调光的情况下,测试CSH脚位电压,使用万用表负极搭在板子上的负极,测出电压1.19V左右,如果万用表负极搭在直流电源负极时,测出CSH脚位电压就在1.24V左右,这种情况是不是板子有干扰吗

  • Hi
    1。 不影响。
    2. 从你的描述看是noise问题造成的? 建议你layout上严格区分模拟GND和功率GND, 类似CSH这类脚都是用模拟GND的。