请问:
LM3424 DIM引脚通过PWM调光接线
PWM信号是直接 接入nDIM引脚,还是接入到R4电阻的左边 (如下图)
还是说当接入PWM信号后,就不需要R4电阻了。PWM信号可以直接 接入nDIM引脚。
麻烦协助。
此处PWM应该是电压型的吧。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问:
LM3424 DIM引脚通过PWM调光接线
PWM信号是直接 接入nDIM引脚,还是接入到R4电阻的左边 (如下图)
还是说当接入PWM信号后,就不需要R4电阻了。PWM信号可以直接 接入nDIM引脚。
麻烦协助。
此处PWM应该是电压型的吧。
你好
问1: 如果使用PWM调光,占空比最大97%,这样会影响CSH脚位电压吗?
目前测试如果不用PWM调光,电压可以1.23-1.24V之间,如果接入PWM调光 CSH脚位电压就成1.15V左右。
问2: 在不使用PWM调光的情况下,测试CSH脚位电压,使用万用表负极搭在板子上的负极,测出电压1.19V左右,如果万用表负极搭在直流电源负极时,测出CSH脚位电压就在1.24V左右,这种情况是不是板子有干扰吗