This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED为什么要恒流驱动



1、 LED是一个非线性器件,正向电压的微小变化会引起正向电流的很大变化3.3V时为20mALED用三节干电池供电新 电池电压可达4. 5V电流超过100mA大了5很容易烧毁。

2、1W大功率LED,如果正向电压变化10%(从3.4V降低到3.1V,会引起正向电流从350mA降低到100mA,变化3.5倍。

 

3、LED是一个半导体二极管,它的伏安特性随温度而变化(-2mV/oC)假如用恒压电源供电:温度增加至85,正向电流从20mA增加至35-37mA,而亮度不增加。温度降低至-40度时,正向电流从20mA降低至8-10mA,亮度降低。所以不能用恒压源供电,而必须用恒流源供电。

由以上可以,LED驱动必须用恒流驱动