This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2733X采用5V升12V的方案,负载不够



您好!

LM2733X采用5V升12V的方案,用在线工具生成的电路图输出电流为0.2A,但是实际测量只能达到0.125A,最大负载工作时,芯片温度能够达到50℃。查阅技术手册时发现,技术手册中的输出电流可以达到330mA。不知是什么原因导致我的电源板负载与在线仿真还有数据手册的差距这么大。

下图为手册中的截图: