This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教bq78350电量计学习成功后,FCC每次循环增大问题。

Other Parts Discussed in Thread: BQ78350

bq78350电量学习成功Max Error 2%后,电池连续做了3个循环,每次循环FCC都会增大。

电芯用的磷酸铁锂电池,每次充电差不多满电时,电压上升得很快,所以每次都会触发过充保护,VCT并没有检测到。

CEDV原来设置了EDV_CMP, 因为我们出货电量都在50~60%,带载时电压拉得比较低,电量会在22%~40%间跳变到7%,所以改用VFLT_EN和FIXED_EDV0。

经过几个循环测试,电量跳变的问题是解决了,但是又出现了FCC增大的问题,电池FCC更新后,充电就不能充到100%了,每个循环会下降2%,3个循环就变成95%了。

请教如何改善此问题?