This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

采用TPS65130设计的输出正负12V电压,负电压输出实现不了



你好,我是按照datasheet和user guide上设计的原理图和布局,附件里有我的原理图,不一样的只是将AGND和PGND采用的是磁珠相连接。

现在发现VPOS可以正常输出12V,而负极VNEG输出的则为3.33V,经过测试,VREF=1.22,而VFBP=1.40V,我看手册上写的VFBP应该是0V,为什么这里会有电压? 另外芯片背面有发热现象。

希望可以回答我的问题,谢谢