This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,项目上有个 TYPEC接口充电/USB通讯 需求如下,咨询设计方案:
1.手持设备,电池为锂电池2节或3节串联。产品空间稍大,芯片体积不限,尽量不考虑BGA封装;
2.TYPEC充电,需兼容市面上常见的PD、QC等等协议的手机/笔记本快充充电器、车载充电器、也需兼容以前的慢充充电器、并且能够根据充电器的输出功率调整合适的充电电压和电流;
3.可以和电脑进行USB2.0通讯;
(有点类似支持TYPEC充电的笔记本电脑内部的充放电管理/USB通讯的功能;手机的基本都是3.7V电池的,没法参考手机充电方案)
问题:
1.我们有升降压型的充电芯片BQ25703方案,以前的应用场景是使用确定的充电器,所以根据充电器的输出功率/电流,调整合适的固定的充电电流,没有问题。但是现在新的应用上需要适配不同输出功率的充电器,要考虑充电功率最大化,且不能超出充电器额定功率,不太明白需要怎样的接口芯片或者方案,去设置快充充电器输出5V、9V还是12V,还有怎样去检测充电器的输出电流能力,再去设置充电芯片的合适的充电电流。
2.看过赛普拉斯的TYPEC接口方案,有的芯片是有PD协议,但我自己学识不够,看不太懂,没有找到合适的方案。
3.在TI官网上看到“USB Type-C™ 控制器”、“USB PD 控制器”,感觉可能比较合适,两者有什么区别,分别有什么适用场景吗?
4.在论坛里看到有使用TPS65987D+BQ25703做TYPEC充电方案的,感觉和我的应用场景比较符合,参考设计是TIDA-01627,为啥现在已查不到此设计了?是有新方案代替了,还是涉及保密性所以删除了?
5.必须使用单片机去设置IIC寄存器才可以使用吗?TPS65987D芯片还需要烧写固件才能用吗?
以上,提前感谢!