一些电路中,看到双运放组成的双环反馈,这种组合一般应用于什么场合?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LED路灯电路必需要有恒流功能,以保证LED路灯长久使用。众所周知LED路灯的芯片在高温下LED的导通电压会下降,如果仅用有恒压功能的电源电路,将使LED路灯的电流随时间而增大,因而减少了LED路灯的使用寿命。如果LED路灯电路采用恒流电路,由于目前市面上的恒流开关电源均为低压大电流,所以必需采用多路并连,亦即目前市面上有的电路采用8个、12个或14个LED串联后再并连的方案所组成的驱动电路,由于无论每组8个或12个或14个,每组的导通电压不一,亦即并联后每组的电流分配不均,长期使用后会造成电压低的一组电流分配较多而提前烧毁,进而造成各组被逐个烧毁。
你指的应该是均流吧 ?
明月光 说:LED路灯电路必需要有恒流功能,以保证LED路灯长久使用。众所周知LED路灯的芯片在高温下LED的导通电压会下降,如果仅用有恒压功能的电源电路,将使LED路灯的电流随时间而增大,因而减少了LED路灯的使用寿命。如果LED路灯电路采用恒流电路,由于目前市面上的恒流开关电源均为低压大电流,所以必需采用多路并连,亦即目前市面上有的电路采用8个、12个或14个LED串联后再并连的方案所组成的驱动电路,由于无论每组8个或12个或14个,每组的导通电压不一,亦即并联后每组的电流分配不均,长期使用后会造成电压低的一组电流分配较多而提前烧毁,进而造成各组被逐个烧毁。
明月光 说:LED路灯电路必需要有恒流功能,以保证LED路灯长久使用。众所周知LED路灯的芯片在高温下LED的导通电压会下降,如果仅用有恒压功能的电源电路,将使LED路灯的电流随时间而增大,因而减少了LED路灯的使用寿命。如果LED路灯电路采用恒流电路,由于目前市面上的恒流开关电源均为低压大电流,所以必需采用多路并连,亦即目前市面上有的电路采用8个、12个或14个LED串联后再并连的方案所组成的驱动电路,由于无论每组8个或12个或14个,每组的导通电压不一,亦即并联后每组的电流分配不均,长期使用后会造成电压低的一组电流分配较多而提前烧毁,进而造成各组被逐个烧毁。
说的很仔细,问题都说到了,解释的很清楚