This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25570EVM评估版的输出电压可以改吗?



bq25570EVM评估版上的R10和R9导致输出电压只有1.8V,但是我看文档最开始说

The boost charger output is configured to deliver up to 4.2-V maximum voltage to its output, VSTOR, using external resistors.

升压可以达到4.2V以上,这两个点在一起没明白,能不能帮忙解释一下呢?谢谢