This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050学习不成功

Other Parts Discussed in Thread: BQ4050, GPCCEDV

尊敬的TI工程师:

我有一个4S的磷酸铁锂电池BMS项目,需要用到BQ4050,我按照TI官网给的资料,制作了电路板、并且配置好了相关参数。各种保护功能都正常,充放电了几个回合就是学习不成功,不知道什么原因,麻烦您给看看。

与学习有关的参数配置如下:

1)设计容量:4000mAH

2)设计电压:12.8V

3)充电方式:CC/CVCC=2ACV=14.4V,充电结束电流=0.1A,充电完成以后搁置2小时再放电。

4)放电方式:恒流放电,放电电流=0.8A,放电完成以后搁置5小时再充电。

5Charge Term Taper Current=0.25A

6Charge Term Voltage=0.15V

7FD Set Voltage Threshold=TD Set Voltage Threshold=2.8V

8EMF=14124,C0=690,R0=4,T0=6972,R1=1,TC=11,C1=0(根据TI发来的电子邮件)

是不是我的设置不正确,或者学习方法不正确,期待您的指导,有没有这一方面的资料,麻烦您给推荐一下,谢谢您的指导!

dong1685@163.com