Other Parts Discussed in Thread: TPS75003
TPS75003电源模块调试,1.2V,2.5V输出为1.24,2.54,但3.3V电压输出直接到5.04V!
都是按着文档推荐画的PCB,
现在只焊接了电源模块,没有负载
测试正确的1.2V的p-mos,G极电压、S极电压均约为5V
测试错误的3.3V的p-mos,G极电压3.9V、S极电压均为5V。。。
实在不知道为什么了。。。焦头烂额
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS75003
TPS75003电源模块调试,1.2V,2.5V输出为1.24,2.54,但3.3V电压输出直接到5.04V!
都是按着文档推荐画的PCB,
现在只焊接了电源模块,没有负载
测试正确的1.2V的p-mos,G极电压、S极电压均约为5V
测试错误的3.3V的p-mos,G极电压3.9V、S极电压均为5V。。。
实在不知道为什么了。。。焦头烂额
Yanfeng Liu 说:现在3.3的输出是5V,所以经过分压后FB2的输入时1.8V。。。如果输出时3.3V的话,本来应该约等于1.2V吧。。
你说得没错,如果环路正常工作,FB的电压应该是1.2V。
Yanfeng Liu 说:嗯,只能等上班了去换个mos试一下。。不过是刚刚焊的板,一般损坏的几率不大吧
你可以用万用表量一下PMOS的体二极管还在不在的方法判断是否是MOS损坏。
量一下栅极到源,到漏是否短路,还有一个方法确定PMOS是否损坏就是交换1.2V和3.3V两路的PMOS,看能否正常输出电压,先排除是MOS的问题,再进入下一步的Debug。
Yanfeng Liu 说:嗯,谢谢指导~~~
还有3.3V的pmos的G极(芯片的sw2)是3.9V,S是5V,所以Vgs一直小于0.。。。其实,看了半天芯片一直没明白sw2到底应该是个什么
你用万用表测的SW1和SW2吧?
SW1和SW2的波形应该是开关波形,用万用表测到的是其平均值。
我严重怀疑你把SW1和SW2记录错了,因为1.2V的输出那一路的栅极,应该是占空比为~80%的方波(因为是驱动PMOS管,(5-1.2)/5=77%), 所以你测到的电压约为3.9V=77%*5V.
而你测到的另一个栅极,直接是5V。因为输出电压高于设置的电压,PMOS管不开从控制上也说得通。所以PMOS管损坏的可能性很大。