This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95问题

Other Parts Discussed in Thread: BQ40Z50

您好!充满8.4V,2节18650电芯中,低温放电,终止电压6V,6.9V左右会自动停,电压乱跳,请问是什么原因引起的呢?会跟配置有关吗,以下是我们的配置,请帮忙看配置合理吗?

  • 您好,如果用的是正常放电电流,放电时电压跳变更AFE的参数设置无关,AFE设置的是1段保护的值。
    这款芯片已经不推荐在新设计使用,推荐看一下BQ40Z50
  • 谢谢您的回复,这个是老产品突然遇到的不良问题,不是新设计使用,我们用的电子负载2600ma放电,电子负载可能干扰的电流很大,造成afe保护。在常规正常温度或低温下放电,出现电池电压没有到我们设定的放电终止电压6V之前就无规则随之出现放电终止现象,导致放电容量不达标,但实际电池内部电压没有到最低电压。猜测是哪个参数配置不合理导致,请帮我们分析一下,或提供能够输出导致提前放电终止的相关配置参数。我们目前用的是2串电池,容量13AH与24AH二种规格。
  • 烦请您帮忙解答下,感谢!目前电池问题现象,一块电池在短路实验之后,出现电压跳动,电压一会有,一会无,间隔大概一秒。通过上位机看,一会正常,一会不正常。也是间隔一秒。如图。另外低温下有3个电池放电中途停下,用上位机执行41复位后,同样出现短路实验不正常一样的状态。请问一下什么原因。就这个两个状态一直变. 所有这种现象在重新写data flash后均恢复正常.

  • 您好,可能是做短路测试导致的参数混乱,这种情况只能通过重新烧录固件或者参数解决。