This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50使用过程中,RSOC跳0%

Other Parts Discussed in Thread: GPCCHEM

电池已经选对CHEM_ID,并做过 discharge-relax-charge-relax-discharge的学习。

2节电芯电池,Term voltage设置为6V  Term Cell voltage设置为3V

正常使用过程,约5A放电,在7.1V时,RSOC由39%变为0%。

请问有哪些情况会使RSOC出现为0%,我们现在这个属于量产电池,有用户出现跳RSOC突变0%这种情况,需要确认什么情况下RSOC会突变为0%。以及如何预防跳变问题。