Part Number: LM3880
To whom it may concern,
I am planning to use two of LM3880 to control the power sequence for Xilinx Kintex FPGA.
The power source of PCB is 12V 10A, and I am using that power source to generate 1.0V, 1.5V, 1.8V, 2.0V and 3.3V
Since the maximum input voltage of LM3880 is 5.5V, can I use few resistors to form a voltage divider to turn the 12V power source to 5V as VCC for LM3880?
Is that going to be okay for me to use LM3880 like this?