This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3880: LM3880 with 12V power source

Part Number: LM3880


To whom it may concern,

I am planning to use two of LM3880 to control the power sequence for Xilinx Kintex FPGA.

The power source of PCB is 12V 10A, and I am using that power source to generate 1.0V, 1.5V, 1.8V, 2.0V and 3.3V

Since the maximum input voltage of LM3880 is 5.5V, can I use few resistors to form a voltage divider to turn the 12V power source to 5V as VCC for LM3880?

Is that going to be okay for me to use LM3880 like this?