This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: Battery Charge

Part Number: BQ25792

使用BQ25792給電池充電,出現以下問題:

1.Fast charge current設置為1.5A,同一塊電池(每次充電起始電壓都在2.8V~2.9V左右)不同時間充電時CC mode充電電流不一樣,電池電壓在3.0V以上充電電流有時是100mA有時是300mA有時是1.5A

2.Fast charge current設置為1.5A,幾塊不同的電池從2.8V左右開始充電進入CC mode後充電電流也不都是1.5A

3.BQ25792寄存器設置如下:

  REG00 0x04
  REG01 0x1A4
  REG03 0x96
  REG05 0x2F
  REG06 0x12C
  REG08 0xC3
  REG09 0x05
  REG0A 0x23
  REG0B 0xDC
  REG0D 0xBB
  REG0E 0x39
  REG0F 0x22
  REG10 0x80
  REG13 0x01
  REG14 0x1E
  REG17 0x7A
  REG18 0x14

4.電路圖如下:

以上,請協助確認下原因,感謝~~

  • 您好,发生这种情况时,能否抓一下 VSYS、VBAT、IBAT 的波形?

  • 您好,我有抓取以下兩種情況的波形,

    1.電池電壓3.1V左右時:  ch1:VSYS   ch2:Vbat  ch3:Ibat

    充電電流為70mA左右,而且還不穩定,VSYS只有3.8V

    2.電池電壓充到3.16V時,有更換一個4.1V左右的電池確認充電電流,波形如下:

     

    3.重新插入剛剛充到3.16V的電池,充電電流為1.46A,反復插拔USB及電池,充電電流一直是1.5A左右,無異常,此時VSYS電壓為4.2V左右

    以上,請協助確認,感謝~~~~

  • 您好,您的问题E2E 已经回复,请继续关注。

    https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1006952/bq25792-battery-charge