This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2897A: UCC2897A反复重启没有PWM波,开环没接次级没接变压器

Part Number: UCC2897A


SS引脚只有三角波峰值2.5V  ss电容220nF            把变压器拆了 所以没有过流,因为把过流短路到地上了.           过压保护也是短路到地上了                输入25V  欠压保护电阻上面68K  下面5.1K  欠压保护应该不是    也是有1.9V以上

Vref5V  FB5V

VDD PVDD短路  然后外接2uf电容器   使用官方推荐的mos电路供电  副边绕组没接  现在是10.5V  

为什么一点 PWM都没有