This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53015: 求助: 电源轻载时SW出现震荡,电感啸叫,正常负载或者重载SW波形正常

Part Number: TPS53015


TI的专家们,你们好

最近在用TPS53015进行设计,输入7~26V,输出5V8A

原理图如下:

layout如下:

现象 : 芯片正常工作,但是当负载<2A时,SW波形会出现震荡,电感出现啸叫

             >3A时,SW波形正常

             2A<V<3V时,SW波形出现轻微震荡

空载波形->2A: 

2A->3A 部分震荡波形:

>3A 波形正常:

请教一下专家们,应该怎么去改善SW的波形,非常感谢~