This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5001: 短路时频率升高,输入功率严重加大

Part Number: LM5001


设计条件:

输入电压: 8-42VDC

输出:19V 0.084A   ( Po=1W ) 

效率:80%

拓补:反激  (光耦+431)

用LM5001SD做了两个版本。

第一个版本,室温下输出短路时开关频率维持在100KHz左右,此时输入功率(1.8W)没有明显异常,短路时SW的峰值也可以。

第二个版本,考虑到第一版个别元件封装不合适需要调整,重点挪了SW的吸收用途的RCD的位置,室温下短路时发现输出短路时SW频率升至400KHz ,输入功率到达4W

问题:

1. 第二个版本,为什么短路时频率会升高,输入功率严重加大 ?

2. 第一个版本,在+85C环境中短路时,个别也出现输入功率严重加大的情况 ,是什么原因 ?

3.出现这种问题 是不是 LM5001损坏了?