This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5060: 关于LM5060的GATE引脚和VOUT引脚电压的问题

Part Number: LM5060


根据LM5060内部结构图可知,GATE和VOUT引脚之间有一个16.8V的稳压二极管。

第一个问题:请问是不是,如果达到稳定的状态(即VIN=VOUT)的时候,GTAE对VOUT的电压一定会被稳压二极管钳位在16.8V?

第二个问题:如果外置的MOS的Vgs-max是10V,是不是在电路稳定状态(即VIN=VOUT)的时候,这个MOS管会被损坏?