This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据LM5060内部结构图可知,GATE和VOUT引脚之间有一个16.8V的稳压二极管。
第一个问题:请问是不是,如果达到稳定的状态(即VIN=VOUT)的时候,GTAE对VOUT的电压一定会被稳压二极管钳位在16.8V?
第二个问题:如果外置的MOS的Vgs-max是10V,是不是在电路稳定状态(即VIN=VOUT)的时候,这个MOS管会被损坏?
HI
最高钳位在16.8V,但是实际上可能并不会这么高电压,MOS的导通电压并不会这么高,这里的实际电压你可以测量下。
如果一个MOS的Vgs(th)是3V,按照LM5060的启动工作时序,LM5060会把MOS的Vgs首先充电到5V。请问那之后Vgs的电压会达到多少呢?
Hi
见规格表正常12V+/-2V.
您说的这个参数是datasheet上P6页上的VGATE的参数吧。
我认为这个参数或许是没有参考性的。因为这个参数的条件是“GATE pin open”
如果是外部有一个MOS连接到GATE的引脚上,在IC正常工作下,GATE对VOUT的电压应该是多少呢?
还是在这个范围,具体你可以实际测试一下。