This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62130: 下图是我们的设计原理图,在进行DC12v插入的瞬间,VCOM端和+3.3V处出现电压震荡,具体测试波形如下(电源芯片不工作情况下)

Part Number: TLV62130

其中:黄色为VCOM(电压12V)波形,蓝色为+3.3V波形,可以看出3.3V的震荡电压高达30V,而12V的电压只有10V左右;

请问造成这种情况的原因是什么?这种情况如何去消除或者优化?

  • Hi
        输入电感要去掉的,并且在输入增加较大功率的TVS管保护下。

        不建议操作上12V直接插入,相当于带电插拔(硬开关)开关启动,在输入是会造成电压spike, 特别是还有个电感会更加恶化。