This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61023: 求助:TPS61023总是烧掉

Part Number: TPS61023

我使用TPS61023,输入是电池大约2~3.2V,输出设置为3.1V;负载一般最大300mA。

设计是参考WENENCH提供的参考设计。

最近发现,使用新电池,大约Vin会略大于输出,平时使用还OK;在驱动蜂鸣器和LED频闪的时候,总是会芯片烧毁,电感甚至发烫的熔锡;我测试了一下电流顶过10mA来回变,应该不存在过流问题;

用示波器抓到烧毁瞬间,VIN没有变化,但是VOUT会冲到4.6V,然后就烧毁了。求教可能是什么原因?

黄线是VIN,蓝色是VOUT