Other Parts Discussed in Thread: BQSTUDIO, GPCCEDV
Hi,你好:
目前我们在使用bq27220的时候碰到一个奇怪的问题:放电过程中RSOC异常hold在14%。我们有测试出6+次这种现象,不同设备,不同gmfs都有出现。具体复现流程和现象如下:
流程:
- 取一块满电的电池(DC 1500mAh)插入我们的设备,给设备和bq27220上电;
- 将我们校验后的golden image(bqstudio 产生的gm.fs)通过CFG_UPDATE写入bq27220中;
- 开始-100mA恒流放电;
现象:
- 100%到15%时放电曲线正常,即每个ROSC点停留10分钟左右,但到了14%时,异常停留90分钟+,而后直接drop到7%(到达EDV2 thredhold)。
请问出现这种异常的原因是什么,是不是算法在14%时有什么特殊的处理?