This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27220: 放电过程中RSOC异常hold在 14%

Part Number: BQ27220
Other Parts Discussed in Thread: BQSTUDIO, GPCCEDV

Hi,你好:

     目前我们在使用bq27220的时候碰到一个奇怪的问题:放电过程中RSOC异常hold在14%。我们有测试出6+次这种现象,不同设备,不同gmfs都有出现。具体复现流程和现象如下:

     流程:

  1.      取一块满电的电池(DC 1500mAh)插入我们的设备,给设备和bq27220上电;
  2.      将我们校验后的golden image(bqstudio 产生的gm.fs)通过CFG_UPDATE写入bq27220中;
  3.      开始-100mA恒流放电;

     现象:

  •      100%到15%时放电曲线正常,即每个ROSC点停留10分钟左右,但到了14%时,异常停留90分钟+,而后直接drop到7%(到达EDV2 thredhold)。

       请问出现这种异常的原因是什么,是不是算法在14%时有什么特殊的处理?

  • 您好,您用的是fix CEDV还是CEDV算法,请确认CEDV的参数是否配置,看一下GPCCEDV的报告中计算的参数是否合适。

  • 你好

           我们用的是CEDV算法,这种现象的复现率是40%左右,所以GPCCEDV的报告中计算的参数应该是合适的,不然复现率应该为100%,不知道我这样理解是否正确?

           另外假如GPCCEDV的报告中计算的参数不合适,为什么会,hold 14%,而不是15%,18%或者其它相近的值,还请告诉我们理论根据。因为我们从《BQ27220 Technical Reference Manua.pdf》中了解到,会hold RSOC的地方只有EDV2/1/0(7%,3%,0%)这三个地方。

    谢谢

  • 您好,是否方便提供一下放电的log数据和GPCCEDV的报告。