This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1205: LMG1205在100K开关频率下驱动EPC2053发热严重

Part Number: LMG1205


我们用LMG1205驱动EPC2053组成的半桥,开关频率微100KHZ,死区时间为100ns,驱动电阻为2欧姆,发现LMG1205和EPC2053在空载(半桥中点不接任何负载)下发热特别严重(LMG1205和EPC2053都发热严重),温升高达25℃,希望TI工程师给出导致发热的见解,感谢。

  • Hi

           主要注意驱动电压是否有波动超过6V, 其次就是注意驱动和晶体管的焊接,例如EPC2053,  如果是junction to ambient 热阻就高达53℃/W,  需要junction to  case/board 可以实现非常小的热阻。驱动芯片也一样,建议注意。

           其次芯片温升过高,还要注意duty控制,电路异常到晶体管异常工作也可能造成温度过高。