This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78Z100: CBTime1 CBTime2

Part Number: BQ78Z100

Hi 您好

1. 參數開啟 CB=1 CBR=1

  CB 是在在充電狀態中平衡   

  CBR  單獨對Cell 平衡  也就是靜態平衡  , 那放電過程中是否也會平衡

2. CB Tim 

   是怎計算的  , 會累計?   Cell 電壓差是差多少 開始平衡

3. 0X0076 是否會讀取 CBTime1  CBTime2

* 請查收資料

F10NG1.rar

  • 您好

    1,放电不会平衡。

    2,平衡时间请参考下面的公式

    Bal Time/mAh Cell 1 = 3600 mAs/(VCELL/RVC1 + Rcb) × DUTY/1000

    Bal Time/mAh Cell 2 = 3600 mAs/(VCELL/(RVC1 + RVC2 + Rcb) × DUTY)/1000

    Where: VCELL = average cell voltage (for example, 3.7 V for most chemistry)

    RVC1 = resistor value in series to VC1 input (for example, 100 Ω, based on the reference schematic)

    RVC2 = resistor value in series to VC2 input (for example, 5 Ω, based on the reference schematic)

    Rcb = cell balancing FET Rdson, which is 150 Ω.

    DUTY = cell balancing duty cycle, which is 66% typ.

    Cell balancing time for each cell to be balanced is calculated by: dQCelln × Bal Time/mAh Cell 1 for cell1 or and dQCelln × Bal Time/mAh Cell 2.

    3,此命令返回的是正在平衡的电池的状态。

  • HI Star

    在請教一下 CBR=1 針對單串靜置平衡

    Bal Tim2 啟動居多 , 但電芯壓差都在20mV 以內

    平衡條件啟動是什  也就是不會看電芯壓差  時間到就會啟動對吧

    Pega F10 2021.09.08 6PCS.rar

  • 您好,CBR=1应该是在relax mode进行balance

    balance启动条件请参考TRM 7.3 Cell Balancing Operation

  • HI Star

    在跟您請教一下  Min Rsoc for Balancing 設定80%

    CBR=1 RSOC<80% 不會啟動靜置平衡  我的理解正確嗎

  • 您好,Min Rsoc for Balancing 設定80%,如果小于80%不会启动平衡。

  • 最後請教 

    1. Relax Balance Interval 18000s 約12.5h   是指這段時間再運作靜置平衡

    超過這時間  將重新計算

    2. 假設CBTime2 累計10000秒 只要充飽電 就會歸0  對嗎

  • 您好

    1,是的,在Interval时间内进行balance

    2, The cell balancing time is stored in the 16-bit RAM register CellnBalanceTimer, providing a maximum calculated time of 65535 s (or 18.2 hrs). This update only occurs if a valid QMax update has been made; otherwise, they are all set to 0.

  • HI Star

    1. 當 CB Tim 1  CB Tim 2 其中一個有紀錄時 除非數據很少只有幾千 才有 可能在充電過程中CB 完全平衡 讓數據歸0

    2. CB Tim 1  CB Tim 2 在靜置時 壓差 <3mV設置 不管RS0C設定80% 它會慢慢歸零

    3. 如果Cell > 3mV 紀錄就會一直累計或停留 在那 對吧

    下面是我測試的數據與報告  是否正確

    Kili CB Tim TEST 2021.09.10.ppt

     

  • 您好, 为更加有效地解决您的问题,建议您将问题发布在E2E英文技术论坛上https://e2e.ti.com/support/power-management/f/196

    将由资深的工程师为您提供帮助。我们的E2E英文社区有TI专家进行回复,并得到全球各地工程师的支持,分享他们的知识和经验。