Hi 您好
1. 參數開啟 CB=1 CBR=1
CB 是在在充電狀態中平衡
CBR 單獨對Cell 平衡 也就是靜態平衡 , 那放電過程中是否也會平衡
2. CB Tim
是怎計算的 , 會累計? Cell 電壓差是差多少 開始平衡
3. 0X0076 是否會讀取 CBTime1 CBTime2
* 請查收資料
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi 您好
1. 參數開啟 CB=1 CBR=1
CB 是在在充電狀態中平衡
CBR 單獨對Cell 平衡 也就是靜態平衡 , 那放電過程中是否也會平衡
2. CB Tim
是怎計算的 , 會累計? Cell 電壓差是差多少 開始平衡
3. 0X0076 是否會讀取 CBTime1 CBTime2
* 請查收資料
您好
1,放电不会平衡。
2,平衡时间请参考下面的公式
Bal Time/mAh Cell 1 = 3600 mAs/(VCELL/RVC1 + Rcb) × DUTY/1000
Bal Time/mAh Cell 2 = 3600 mAs/(VCELL/(RVC1 + RVC2 + Rcb) × DUTY)/1000
Where: VCELL = average cell voltage (for example, 3.7 V for most chemistry)
RVC1 = resistor value in series to VC1 input (for example, 100 Ω, based on the reference schematic)
RVC2 = resistor value in series to VC2 input (for example, 5 Ω, based on the reference schematic)
Rcb = cell balancing FET Rdson, which is 150 Ω.
DUTY = cell balancing duty cycle, which is 66% typ.
Cell balancing time for each cell to be balanced is calculated by: dQCelln × Bal Time/mAh Cell 1 for cell1 or and dQCelln × Bal Time/mAh Cell 2.
3,此命令返回的是正在平衡的电池的状态。
您好
1,是的,在Interval时间内进行balance
2, The cell balancing time is stored in the 16-bit RAM register CellnBalanceTimer, providing a maximum calculated time of 65535 s (or 18.2 hrs). This update only occurs if a valid QMax update has been made; otherwise, they are all set to 0.
您好, 为更加有效地解决您的问题,建议您将问题发布在E2E英文技术论坛上https://e2e.ti.com/support/power-management/f/196,
将由资深的工程师为您提供帮助。我们的E2E英文社区有TI专家进行回复,并得到全球各地工程师的支持,分享他们的知识和经验。