我买了8个LMG1210芯片,配合EPC8010使用,只有2个能正常输出波形,其他的基本都输出不稳定的波形,就像我一开始描述的的那样(波形时有时无)。正常半桥斩波输出的波形如下我买的8个芯片都是RVRR系列的,另外我想问下RVRR和RVRT这两个系列有什么不一样
还有就是我换了新的MOS芯片(AO6602),使用n沟道的,斩波输出的波形还是一样,一闪一闪的。我测了此时HO的输出波形,也是一闪一闪的(波形时有时无)。布线我也按照案例一样布线,可结果还是一样。我严重怀疑这款芯片(LMG1210)的质量是不是有问题