This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5001: LM5001

Part Number: LM5001

LM5001参照 Figure  20  的设计电路,想要输出42V的电压,

    输入电压给了12V,

   R1用了  75K   的电阻,

   R2用了  7.5K   的电阻, 

   R3用了   55K  的电阻,

   R4用了   75K  电阻,

   R5用了   55K  的电阻,

   R6用了  1.5K  的电阻,

  其他的参数都没变,为什么我的输出电压没什么变化?

   请求大神给予解答,谢谢。