This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC3818: 在调试UCC3818时遇到频繁炸管现象

Part Number: UCC3818
Other Parts Discussed in Thread: UCC28070

在调试UCC3818时遇到频繁炸管现象,无解。电路图使用的手册上推荐的电路图,改进了驱动。意图调试正常输出后再调试反馈网络。但是,初次系统一直无法正常的输出400V电压,只有310V,十分困惑请求帮助。附件时电路图。

电源板设计图.pdf

  • Hi

        不建议你驱动8个MOS,即便你额外增加了双晶体管的驱动。一般同时驱动2个就比较勉强,因为你还要考虑layout影响,考虑Vth差异。不同于输出的同步整流,即便导通上有差异,但是因为有体二极管,对于输入端差异影响相对就比较大。

        如果你需要做大功率的PFC,   TI有推荐UCC28070的,datasheet提供了3.5kW的参考设计,甚至并联做四相功率输出更大。

        同时避免启动烧MOS, 一般可以先轻载启动,以及输入源功率限制。

  • 非常感谢!

    Thank you so much!

    Have a good day  ^_^