This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: 启动问题:只出现1个200ns的PWML脉冲,RUN维持高电平时间为160ms,1.44s循环一次

Part Number: UCC28780

专家你们好:

       Vin20V50V都试过了,PWML脉冲的持续时间为200nsIpri电流的峰值在Vin20V时为680mARcs0.165Ω,所以Ipri^Rcs只有0.11V(再加上Ccs和Ropp的延迟,CS检测到的电压比0.11V还小),并没有达到0.28V,按道理PWML的导通时间应该更长(最大2us),如图1所示。

1

RUN高电平持续时间为160ms,每1.44s出现一次,如图2所示。

2

       然后我就把驱动芯片(NCP51530)的供电给断开,这样管子无法开通,CS脚无法检测到电压,会认为CS短路,就出现了如图3所示,可见RUN脉冲持续4usPWML脉冲持续2us,每1.44s出现一次,符合CS短路故障的情况。

3

困惑点:

1.1PWML只持续了200ns就提前关闭,此时Rcs电压还没达到0.28VRUN高电平持续时间从4us变成了160ms,因为此时Vin<Vbrown-in(107V),PWML应该是3个脉冲,但是却只有一个脉冲。

2.前段时间我的电路是可以正常工作的(https://e2echina.ti.com/support/power-management/f/power-management-forum/208996/ucc28780-1-6ms-pwmh-pwml),就是后面突然PWML产生不了,然后我就开始更换UCC28780,其它电路没有改动,换了第8UCC28780才正常工作,但是过了一会又出问题了,接着又换了差不多有10几个UCC28780,还是无法成功。我的热风枪使用的是400摄氏度和300摄氏度,应该不是芯片烫坏的原因。还有就是我的芯片有在淘宝买的,也有在立创买的,但没有买TI官方渠道的,买的是RTER封装,我猜想是不是芯片的控制逻辑容易出问题还是因为我没有买TI官方芯片的原因。

 

谢谢。