This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
是烧USB-TO-GPIO设备,还是烧UCD3138板子?
烧录应该是系统上的问题,建议你在美国E2E上提问: https://e2e.ti.com/
从使用指南中看用的系统的windowxp, 用window10或者其他系统应该是有差异的。E2E上应该有这个设备的工程师可以帮到你。
是烧录UCD3138 IC ,系统一直都是用着WIN7 32位,看第三个情况是 一开始20年的产品拆开产品和目前买的拆开电路板上的电阻是不同的,是否你们的产品更改了电阻导致这样的故障发生,请帮助我解答问题,因为我去不了美国的E2E,打不开尝试很多次了,请帮助我解决问题
是烧录UCD3138 IC ,系统一直都是用着WIN7 32位,看第三个情况是 一开始20年的产品拆开产品和目前买的拆开电路板上的电阻是不同的,是否你们的产品更改了电阻导致这样的故障发生,请帮助我解答问题,因为我去不了美国的E2E,打不开尝试很多次了,请帮助我解决问题
Hi
放到美国E2E, 国庆节耽误了,很抱歉。
中文论坛和英文论坛一样的操作,比较建议你直接在上面问,主要是具体的问题你来描述会更清楚。
Hi
美国那边也一直没有回复。
我觉得可能是软件的问题,但是我们没法解决,TI在数字电源程序方面TI以前都不提供程序的,也基本上没有任何文档的讲解,一般我们也都是到美国E2E上去问。
您好 我看到你美国发布的帖子有回复了 我给使用部门看下情况 然后针对帖子的信息回复您在给到美国E2E论坛哈 感谢您的帮助
您好 工程师说升级了美国E2E所说的版本 还是一样的问题出现 没有得到解决 您可以帮我回复美国那个帖子么?谢谢你
Part Number: USB-TO-GPIO
Other Parts Discussed in Thread: UCD3138
The newly bought USB-to-GPIO adapter has the following abnormal problem, which has seriously affected the production. Please help forward it TO the supplier, thank you!
1, the same computer, programming procedures, long programming time
For example, the following primary programming UCD3138, the original 10.224 seconds, the new 17.91 seconds. If it is secondary programming UCD3138-064/128, the gap is even larger. (Impact on efficiency),
2.
Recently, the newly bought adapter is very easy to crash, programming more than ten or twenty devices began to crash once, restart the software and normal programming.
Often in the following item on the software automatically quit or error, error report see the attachment.
3.Compared with the adapters purchased on the website for a long time, there are two different versions. Please check the differences marked on the PCB board. Will this affect the use of the product?
4.The failure rate of adapters is high, 3 adapters were damaged during programming today, and there were some damaged before, please inform us of the solution
5.The product has been upgraded, but the problem is still not solved