This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55340: TPS55340

Part Number: TPS55340


大家好:

   我用的TI TPS55340MRTETEP,这颗DCDC,输入电压15V电源供电,输出28V,输出负载的电流需求最大也就1.2A,现在发现输出非常不稳。

  原理图和波形如下,输出28V甚至会冲到42V了,帮忙看看是哪里有问题啊。

  对了,不加负载,输出开路时,输出电压测量是正常的28.3V,一加负载就不行了。

 输出负载是LDMOS PA的 漏极,会PMW 模式的需求电流。

谢谢!