This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于tps61195 pwm控制的问题

Other Parts Discussed in Thread: TPS61195

问题1.tps61195实现pwm控制,那么需要提供pwm脉宽调制信号给tps61195,我想用两个开关分别控制亮度的增加和减少,那么该如何做,是否有合适的脉宽调制芯片可以推荐?

问题2.tps61195一共有8路输出,每一路输出的电流是恒定的,是否意味着每一路串联的灯的数量都要一样?如果其中一路或者两路减少一个串联的灯是否可以通过在减少灯的那一路连接一个电阻来解决?

问题3.有8个开关,分别连接8路线,我想实现按其中一个开关该开关对应的这路线实行接通,同时另外7路线就断开,请问这该如何实现?是否有这样的线路切换开关芯片?

以上问题麻烦专家帮我解答一下,谢谢!

  • 1. 即然是使用PWM调光,可通过调节PWM点空比来调光,没有必要使用两个开关。

    2. 一般输出的串联的灯数是一样的,如果串联电阻会增加额外的损耗;

  • 您好,感谢您的回复,不好意思,我比较菜鸟,所以麻烦您能否详细一点回答我:

    1.使用一个开关来调节,这一点我明白了,但是,开关是无法直接输出占空比信号的,开关应该要连接到脉宽调制信号的芯片吧?然后再通过脉宽调制芯片输出占空比信号到tps61195吧?能否推荐一个这样的芯片给我?

    2.串联的灯数要一样,这个问题我也明白了。

    3.上面第三个问题是否能麻烦您给我解答一下,ti是否有符合我要求的切换开关控制芯片可以推荐?

  • 问题1:PWM可以通过类似555或者一个简单的MCU给出

    问题2:TPS61195的输出是恒流控制,即使一个通道少一颗灯,电流也可以恒住,只是芯片相应通道的压降变大,功耗增加。最好各个通道的灯数一致。