Part Number: BQ76952
BQ7695202 IC 充电和放电的驱动电压没有达到设置的电压 只有5V左右 ,设置的是11V模式,测量CP1对BAT脚的电压也只有5V左右,是电荷泵没有正常工作吗?另外02版本烧录之前转IIC取掉CRC烧录进程序,烧录完后如何转回CRC?
Operation with VBAT up to 80 V is supported when the charge pump is not in operation. Whenever the charge pump is in operation (in
5.5 V or 11 V mode), the maximum voltage on VBAT should be reduced to ensure the voltage on CP1, CHG, and DSG does not
exceed their maximum specified voltage.