This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Charge pump capacitor

Part Number: BQ76952


BQ7695202   IC 充电和放电的驱动电压没有达到设置的电压    只有5V左右   ,设置的是11V模式,测量CP1对BAT脚的电压也只有5V左右,是电荷泵没有正常工作吗?另外02版本烧录之前转IIC取掉CRC烧录进程序,烧录完后如何转回CRC?

Operation with VBAT up to 80 V is supported when the charge pump is not in operation. Whenever the charge pump is in operation (in

5.5 V or 11 V mode), the maximum voltage on VBAT should be reduced to ensure the voltage on CP1, CHG, and DSG does not

exceed their maximum specified voltage.