This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Burst模式

Part Number: UCC28950


目前在做一个3KW的电源,220输入,输出48V,100K的频率,有些问题请教一下:

1.请问在空载的时候进入Burst Mode的话,输出电压波形是不是像图1一样有很多脉冲干扰?

2.看了规格书,Burst Mode只能调RTMIN来设置,我都调到规格书说的最小13K了,还是会进入Burst Mode,有什么好方法能够解决吗?

3.需要什么资料可以说一下,上传给你。

                                           图1